Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Si1102 and Si1120 Slide 21
An earlier slide showed a single LED implementation where the TXO signal was used to directly control a single LED. Here is another application example where the Si1120 is used, in conjunction with an MCU, to control three IR LEDs which may be useful for motion, position sensing (XYZ) or other similar functions (IR sliders). Each LED is gated through an external gate that is enabled on a time multiplexed fashion by the MCU. For example, in the figure, the P2.1 signal, when high, enables the TXO signal to sink current from the D1 LED through Q1. The other two GPIOs shown (P2.2 and P2.3) would leave those gates disabled while the D1 LED is used. On the next cycle the P2.1 I/O is de-asserted and the P2.2 I/O is asserted causing the TXO signal to sink current through the LED connected to Q2. This cycle repeats for the remaining gates and diodes in the system. The Si1120EK includes a board that implements this three LED scheme and this schematic is a representation of that system.
PTM פורסם ב: