Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Si1102 and Si1120 Slide 15
Shown here is a block diagram of the Si1120. The analog front end consists of two photodiodes that measure the incoming electromagnetic energy. One of the detectors is used to measure the IR energy and the other is used to measure the energy in the visible spectrum. The complete analog signal chain is integrated and provides the low going PRX output which is a pulse proportional to the light intensity. The TXO output is a constant current sink that can be set to 50mA or 400mA (with no current limiting) in order to directly drive an IR LED for the emitter. STX, SC and MD are control inputs to set the operating mode and STX also starts the conversion process.
PTM פורסם ב: