Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Si1102 and Si1120 Slide 7
Designers of devices that implement IR proximity detection need to be concerned with several items. First and foremost the detection range must be determined. In order to detect the reflected energy, the object must be within range of the IR energy source. When determining the proximity range the IR energy output must be set in order to accommodate the decrease in light which is proportional to the inverse square of the distance. Taking into account that the light must travel in the transmit and receive path, the energy that the detector sees is inversely proportional to the fourth power of the distance from the emitter.
PTM פורסם ב: