Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Si1102 and Si1120 Slide 19
Now that the mode is set, the Si1120 can start being used to take IR proximity measurements. The STX pin is now used as a source to start the measurement and can be controlled by the MCU hardware (by using timers) or by firmware. When the STX line is driven high the measurement cycle begins. At the time the STX goes high, the Si1120 takes the ambient IR reading and stores this for later. After the ambient measurement, the TXO signal is driven low which then starts the constant current flow through the LED. During this time when TXO is asserted, the Si1120 actually measures a combination of ambient IR plus the reflected IR. To get the reflectance, the Si1120 subtracts the ambient IR measured at the beginning of the measurement cycle from the overall measurement when the LED is emitting the IR energy. If the accuracy of the measurement is not required, for example when doing a simple threshold detection, then a measurement cycle can be aborted by bringing the STX line low again, thus raising PRX and TXO. This can reduce overall power consumption by minimizing the pulse width outputs.
PTM פורסם ב: