Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Si1102 and Si1120 Slide 17
The Si1120 has seven operating modes that range from measuring the ambient light to the reflected IR as well as determining the output LED drive current from the TXO pin. PRX400 is best for range, PRX50 is best for power saving (PRX50H is not generally used). OFC mode is typically used to figure out the minimum PRX pulse width without an LED which is representative of the PRX pulse width during dark ambient conditions since the LED is not turned on. OFC is used more rarely than either PRX400 or PRX50 as it is more like a calibration step and probably is done once every time the system boots and the value is stored in memory. OFC is used to represent what the PRX50 or PRX400 would have reported if there was no reflected IR energy. The PRX400 minus the OFC value, for example, is a more accurate representation of the reflectance. In applications implementing ambient light sensing, VAMB, VIRL and VIRH will all be used equally. However, not all applications will require ambient light sensing.
PTM פורסם ב: