Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Si1102 and Si1120 Slide 28
Shown here is a sample acquisition using the Si1120EK. In this example, the LEDs labeled red, pink and blue are enabled using the jumpers on the board. In the top plot, a hand moves from left to right and then back again. From the figure the designer can see the red and blue traces start at the same time indicating that the Si1120 is receiving the reflected energy from the hand from both LEDs at the same time. The only difference is the magnitude since the blue LED is farther from the Si1120 then the red. As the hand moves to the right the pink LEDs reflected energy starts to get detected as shown by the increase in magnitude. The opposite is true for the reverse direction in the plot. As the hand moves right to left the pink leads the red and blue.
PTM פורסם ב: