Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
Medical ECG Slide 14

One technique that is commonly used to reduce 50 and 60 Hz noise in an ECG system is called right leg drive. The purpose of this circuit is not only for noise reduction, it is also used to provide a common mode reference. If a design uses a single supply of 5 V, the common mode reference will often be biased at mid-supply. The overall goal of this is to establish a common mode mid-point, which in this case is done with the gain resistor split on the front end INA, amplifies it, and feeds it back such that the overall noise seen at the input of the instrumentation amplifier is reduced. Therefore the amplifier has to reject to less noise through its common mode rejection ratio.

PTM פורסם ב: