Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
Medical ECG Slide 29

Patient monitoring and the ECG market will be discussed first. Shown on this slide, beginning at the lower left, are the different market segments which range from low-end, to mid-end, to high end. As the applications progress from low-end to high-end, the number of sensor leads increases. With an increased number of leads, there is a corresponding increase in the complexity of the analog circuitry, MCU, signal processing, and power requirements, which are going to affect each of these markets. As an example, on the low-end, there are heart rate monitors, consumer instruments and PBANs, personal body area networks. The mid-end applications include pulse monitors, defibrillators, and other types of patient monitoring. Finally, the high-end market includes instruments such as ECG, EEG, fetal ECG, and bispectral index monitors.

PTM פורסם ב: