Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
Medical ECG Slide 22

The block diagrams shown on this slide are laid out for both signal paths, high resolution and low resolution. Overall, one thing that will be seen is that if the user’s choice is the over-sampled approach, there can actually be a reduction in hardware and filter requirements resulting in a lower system cost, and the actual electrode offset information can be retained. Many times, in the discrete solution with a SAR converter, this cannot be done because it is necessary to filter out the electrode offset information with a high pass filter.

PTM פורסם ב: