Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
Medical ECG Slide 2

The ECG has progressed a long way. Shown on this slide is Willem Einthoven’s first practical electrocardiogram, which was developed in 1903. As can be seen, the subject is sitting in a chair with both hands submerged in the first electrodes; these are buckets with a fluid, connected for the right arm, left arm, and left leg. The point of this illustration is that the same function can now be implemented in a much smaller form factor, on a PCB.

PTM פורסם ב: