Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
Medical ECG Slide 8

Before proceeding into the specifics of the electronics, this slide shows the block diagram of the entire system involved starting with the protection circuitry on the front end. That is where the right arm, the left arm, the left leg are input through a lead selection scheme which is going to be differentially sensed by an instrumentation amp and then high pass filtered, amplified, low pass filtered, digitized with an analog digital converter, and communicated to the microcontroller at which point signal processing is going to occur.

PTM פורסם ב: