Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
Medical ECG Slide 15

The right leg drive amp is one of the most complex aspects to deal with in ECG electronics. A large amount of analysis is required to accomplish this correctly. Shown on this slide is a representative sample of the equations involved, showing the effects of the right leg drive amp loop back to the body. One thing to note is that the more gain that is put into the right leg drive amp equates to a better CMRR, the common mode rejection ratio which is a figure of merit in front end amplifiers. The actual overall feedback loop compensates for electrode offsets that are introduced by the body electrode contact.

PTM פורסם ב: