Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
Medical ECG Slide 16

Due to the fact that the right leg drive amplifier is very critical, it is recommended to conduct a very detailed analysis and apply some sort of simulator, such as Spice. Simulating the electrode body contacts is represented in the diagram on this slide with capacitance and impedance in parallel. Because the circuit is an overall loop-on-loop, often customers will integrate a particular device as the right leg drive amplifier and they will claim that this low noise part is in fact very noisy. What the user often does not realize is that it is periodically very noisy, which indicates that the overall loop is oscillating. Maintaining stability in a right leg drive amplifier is a challenge, especially when using single supply devices.

PTM פורסם ב: