Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
Medical ECG Slide 6

Shown on this slide is an example of the signals monitored in an ECG. In the diagram on the left is a typical ECG waveform showing the atrial depolarization and the ventricular depolarization, which is represented by that large QRS interval. On the right is an illustration showing each portion of the heart and the signal that it contributes to the overall ECG waveform. In the top portion the ECG waveform starts at the spinal atrial node and progresses through the atrial muscle, then through the AV node all the way down through the left ventricle, which is the portion of the heart that is responsible for pumping blood throughout the body. The point of this is that by knowing what a normal ECG waveform looks like, it is possible to evaluate an abnormal waveform and allows a cardiologist to diagnose arrhythmias and locate them in specific areas of the heart.

PTM פורסם ב: