Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
Medical ECG Slide 18

Shown on this slide is what a stable signal looks like in simulation. It looks like an inner section between the feedback and the overall open loop gain at 20dB per decade. A problem that can happen in ECG analog front end conditioning has to do with the shield drive. As shown, the shield can be on the order of 500 to 1.5 nF of capacitance. Therefore, when using a very low power, single supply device it can often be a problem driving it directly. Stabilizing the shield drive is also an issue that needs to be strongly considered.

PTM פורסם ב: