Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Product List
Medical ECG Slide 43

In summary, the ECG has progressed a long way since it was developed in the early 1900s. The ECG market can be divided into three segments based on complexity; low-end, mid-end and high-end. As the instruments increase in sophistication the number of sensor leads also increases, creating the need for more complex analog circuitry, MCUs, signal processing and power circuitry. The basic building blocks of the modern ECG include an analog front end, instrumentation amp, high and low pass filters, gain amplifiers and an ADC which communicates with the MCU. Power management is also a major concern in these systems that require stable, noise free power, frequently on multiple rails, for the application.

PTM פורסם ב: