Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Overview-Slide13

In the screen capture shown here, the actual startup of an MSP430 digitally controlled oscillator (DCO) is plotted. It can be seen that from an interrupt event, the DCO is active and stable in well under 1µs – the F2131 DCO startup time is actually 204ns in this example. With the MSP430, clock start up is “instant-on” using the DCO with no delay or 2-speed clock startups. The associated application has instant access to the high-speed DCO from any operating mode.

PTM פורסם ב: