Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Overview-Slide14

A common benefit of an instant-on and stable high-speed oscillator is response to serial communication. For example, the clock source for the UART must start and be stable instantly to prevent received characters from being lost. If a slow or 2-speed oscillator is used, the first character in the received and the data stream is lost. Also, instant-on saves power as the system does not have to waste energy waiting for oscillator startup allowing events to be serviced immediately.

PTM פורסם ב: