Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Overview-Slide32

By combining the flexibility of in-system programmable Flash memory, unobtrusive embedded emulation, and a common user interface, development time is reduced. Also, should the situation arise, last minute code updates as well as remote scheduled and unscheduled upgrades can also be made. Once the project is complete, access to the JTAG port can be permanently disabled using a non-erasable fuse. Spy Bi-Wire, which is another interface only available on new small pin count devices such as the F20xx and F22xx, offers the same real time embedded emulation support but only uses two wires instead of the usual four. This allows for more pins to be used for other functionality instead of being dedicated for debugging support.

PTM פורסם ב: