Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Overview-Slide21

The MSP430-TMP100 measurement system is designed to operate on as little power as possible while continuously displaying the real-time temperature of the TMP100 sensor’s environment. When operated in one-shot mode, the TMP100 goes into shutdown mode after each conversion is completed and consumes a typical current of 0.1uA between conversions.  This, coupled with the energy efficient stand-by modes of the MSP430, which consume a typical 0.9uA in low power stand-by (LPM3) along with a 3.5 digit static LCD, creates a complete temperature monitor and display system capable of 0.5°C resolution while consuming less than 4.93uA total average current.

PTM פורסם ב: