Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Overview-Slide17

The supply voltage supervisor (SVS) is used to monitor the AVCC supply voltage or an external voltage. It has a current consumption of 10uA when active. The SVS can be configured to set a flag or generate a power-on reset (POR) when the supply voltage or external voltage drops below a user-selected threshold. The SVS features include:  AVCC monitoring, selectable generation of a POR, output of the SVS comparator that is accessible by software, low-voltage condition latched and accessible by software, 12 selectable threshold levels, and an external channel to monitor external voltage. Additionally, ADCs support internal Vcc measurement.

PTM פורסם ב: