Maker.io main logo

3D Printed Circuit Boards

226

2023-07-20 | By Lulzbot

License: See Original Project 3D Printing

Courtesy of Lulzbot

Guide by Lulzbot

Description

Inside every modern electronic device, Printed Circuit Boards (PCBs) create connections that allow ‎appliances, computers, and machines to function. PCBs have now evolved to allow for infinite ‎possibilities in any application. In this lesson, our students will be designing and creating their own PCB ‎through the utilization of 3D printers and conductive filaments!‎

Introduction

Lesson Overview:‎

The world of modern electronics and technology would not be what it is today without the invention ‎and consistent innovation of printed circuit boards, or PCBs. ‎

A printed circuit board is a device that creates electrical connections between components that are ‎secured to the PCB. A PCB combines layers of conductive and insulation materials in order to allow ‎electricity to flow in designated paths. Through this real-world design challenge, students will be ‎challenged to create a PCB of their own! ‎

Utilizing an engineering design process, students will identify the roles PCBs play in industry, as well as ‎how they are produced. Students will be able to research and brainstorm different solutions, as well as ‎design their own prototype solution that puts this technology to use! Once designed, students will ‎utilize 3D printers to manufacture custom 3D printed circuit boards as we learn how this modern rapid ‎prototyping technology can combine a variety of materials for infinite possibilities. Understanding how ‎these technologies work, as well as how to create them, are vital skills for any future designer or ‎engineer working to create electronics.‎

Prototype_1

Various 3D printed circuit board prototype examples with a LulzBot TAZ Pro 3D printer

Utilizing an Engineering Design Process:

An Engineering Design Process, or design loop, is a method used by scientists, designers, and ‎engineers to develop solutions to our everyday problems. Through a design loop, students will ‎develop skills in problem solving as they brainstorm solutions and work to create a prototype through ‎hands-on activities. ‎

Design loops come in many shapes and sizes, but none are ever truly ending. The “last” step of any ‎design loop is redesign, or reflection, where we look at what we’ve learned in our developed ‎prototype to improve upon its design. Not being afraid of failure is a powerful concept that leads to ‎greater success and implementation of problem solving.‎

processes

Lesson Objectives:‎

  • Students will be able to identify the benefit of a printed circuit board, as well as how this ‎innovation has impacted the growth of modern technology systems

  • Students will understand the fundamentals of conductivity and how to combine conductors and ‎insulators to make circuit boards

  • Students will combine 3D printed materials with electronic components to make real-world ‎electronic prototype solutions

  • Students will utilize an engineering design process to develop their own solutions to a real-world ‎problem

  • Students will utilize computer aided design (CAD) software to create a 3D model that can be ‎produced on a 3D printer

  • Students will understand how 3D printers work and how they are used in an industrial setting

  • Students will be able to safely apply prototyping techniques to construct designed solutions to real-‎world problems

Materials:‎

This is a list of materials each student will need to complete this lesson:

  • Pencils, rulers, drawing paper

  • Computer or tablet with Internet access

  • Computer Aided Design (CAD) software

  • 3D Printer with both conductive and non-conductive filaments

  • Assorted components to include in prototyping such as batteries, switches, LEDs, resistors, wire, ‎copper tape, motors, and more

  • Click here for sample models shown throughout this lesson

Modifications:‎

In addition to this lesson plan, see our One Page Brief [PDF] that can be used to guide students ‎through the lesson. Additional examples as to how this lesson could be modified are:

  • Additional tools and components to include in fabricating prototypes such as batteries, switches, ‎LEDs, or soldering irons

  • For beginners, providing guidelines in model dimensions or templates to start creating PCBs with will ‎aid in learning CAD

  • Incorporating digital components or micro controllers such as an Arduino or Micro:bit may allow for ‎integration with computer science and additional real-world connections and challenges

  • A dual-head 3D printer is not required for creating printed circuit boards or conductive models, see ‎methods for printing multiple materials with both dual and single extruder printers in the “Printing!” ‎section of this lesson

Considerations:‎

Based upon the age of your students, introduce the concepts of printed circuit boards, electronics, ‎conductors and insulators, and rapid prototyping techniques using terms and concepts familiar to their ‎prior experiences and needs.

‎There is an added challenge when creating PCBs as designs must not only ensure form and function in ‎terms of being able to be 3D printed, but also must consider the flow of electricity in order to function ‎as a circuit board. When working with electronics, special care must be taken to prevent short circuits ‎and damaging components or creating potential hazards when fabricating prototypes. Discuss safety ‎and proper prototyping techniques. ‎

Proper safety procedures should be introduced to students when working in any makerspace or lab ‎environment. When students are around machines such as 3D printers, or using tools to cut or glue ‎materials, students must be informed of potential hazards and taught how to use these resources ‎safely. For reference, see the safety resources by ITEEA. ‎

Assessments:‎

Opportunities for formative assessments will take place through observations and discussions ‎between students as they interact with the content in this lesson. For summative assessment, we ‎recommend utilizing a rubric to assess how a student was able to apply the engineering design process ‎to solve an open-ended problem. Example Rubric - PDF

Essential Questions:‎‎

  • What is a printed circuit board, and how is it used?‎‎

  • Why are both conductive and insulation materials needed for making functioning circuit ‎boards?

  • What components are needed to create a functioning circuit?‎‎

  • How can we use technology to design a solution to a real-world problem?‎

Print_2

When utilizing the dual extruder print head on the LulzBot TAZ Pro 3D Printer,

we are able to ‎print both non-conductive (green spool) and conductive (black spool) PLA filaments ‎simultaneously!‎

Identify the Problem

Electronics and Circuits

Before getting into creating printed circuit boards and their functions, it is important forstudents to have a general understanding of electronics and simple circuits first. In thislesson introduction, cover the topics of electricity, AC vs DC, conductors vs insulators,‎components, polarity, analog vs digital, series vs parallel, and basic circuitry using termsand examples suited to your students’ prior understandings and needs.‎

We suggest you cover the basics of conductivity and polarity by allowing your studentsto get hands-on with fundamental electronic components, like batteries, switches, LEDs,‎and breadboards. Discuss the importance of both conductors and insulators and therelationship between them when creating functional circuits, such as on a breadboard.‎Also discuss the flow of electrons, as well as how to connect safely and properly yourcomponents using batteries and resistors in order to ensure components are not damaged, and ‎short circuits are not created. Using a circuit simulation program like Tinkercad Circuits may allow for students to engage with this content and additional materials online or remotely in a ‎simulated real-world environment.‎

There are endless possibilities in creating electronic circuits and prototype solutions. When ‎using components like lights, switches, motors, or buzzers, students can create anything from a ‎flashlight to an alarm for their lunch box! This lesson introduction will not only offer crucial ‎understandings to foster success in creating printed circuit boards later in the lesson, but also ‎engage and excite your students as they gain greater understandings with items and products, ‎they interact with everyday!‎

Resources:‎

Sample circuits and electronic components for prototyping and exploration.

Objectives:

  • Students will identify the fundamental principles of electricity and how electronic ‎circuits function

  • Students will combine components, conductors, and insulators to create functioning ‎simple circuits

Teacher Instructions:

‎Open discussions to gauge prior understandings of electricity and electronic circuits. Encourage ‎students to explore circuit creation in a safe lab environment. Procedures must be in place to ‎ensure student safety during experimentation. Discuss short circuits and potential risks prior to ‎beginning the activity.‎

Flashlight_3

A prototype flashlight circuit created using analog components and a breadboard.‎

What Are Printed Circuit Boards?‎

With a basic understanding of creating electronic circuits, students may begin toidentify the complexity in modern electronics such as a computer, phone, or 3D printer.‎Challenge students to think how small components must be in order to fit into a smartphone as comparisons is made between the basics circuits they may have created ona breadboard. Most breadboards are around the same size as a smart phone and students may ‎have used a breadboard to make a basic circuit that does one or two things, like a light or an ‎alarm. Imagine how many components and functions a smart phone has, from antennas to ‎cameras, buttons, and a screen, then imagine fitting them all on a single breadboard!‎

This is where printed circuit boards, or PCBs come in! A PCB is a laminated device that ‎sandwiches layers of conductors and insulators in order to make complex circuits fit in compact ‎packages. A PCB is designed by organizing components in locations that correspond to how they ‎need to be connected. PCBs are then fabricated in a variety of methods, from machining using ‎a CNC mill, chemical etching, screen printing, laminating or gluing layers, or even 3D printing! ‎PCBs can also be created to come in all shapes and sizes, as well as both rigid and flexible ‎designs.

‎Nearly every modern electronic device has at least one PCB, from your toaster oven to a car ‎key or your smart phone. Without PCBs and innovations in PCB fabrication, modern technology ‎systems could not exist!‎

Objectives:‎

Students will identify the significance of PCBs, and how they have allowed for technology to ‎evolve over time.‎

Teacher Instructions:

‎It’s difficult to emphasize the significance of PCBs in terms of modern technology innovation. ‎Discuss real-world examples and create connections using terms that suit your students’ needs. ‎Offer examples of how PCBs can be made, as well as the evolution of PCB fabrication in ‎correlation with the demand of modern technology and computing systems.‎

Board_4

This complex printed circuit board is the motherboard from a LulzBot 3D Printer

Without printed circuit boards, modern electronics devices would not be possible. In ‎combination with modern rapid prototyping technology like 3D printers, creating PCBs has ‎never been more accessible for designers and makers like you! To demonstrate these ‎innovations, you will design and create a PCB for a functioning electronic device using ‎computer aided design software and a 3D printer.‎

Specifications and constraints play an important role in a design challenge as they define the ‎limitations and standards that our solution must achieve. For our design challenge, you must ‎abide to the following as you create a prototype printed circuit board solution:

  • You must safely combine conductive and insulation materials to create a PCB‎‎

  • Your PCB must include at least 3 components and perform at least 1 function

  • Your 3D model build volume may not exceed 36 in3

  • You have 1 day to brainstorm, 4 days to build, and 1 day to test & evaluate

Objectives:‎

Students will be able to identify the role specifications and constraints play in a real-world ‎design challenge.‎

Teacher Instructions:

There is no one answer to any solution, nor is there one specific set of constraints for any ‎design challenge. See examples for how to adapt and modify the specifications and constraints ‎of this design challenge under the “Modifications” and “Considerations” section of the lesson ‎introduction.‎

Brainstorm Possible Solutions

Why Solutions and Not Solution?‎

The second step of our Engineering Design Process is “Brainstorm Possible Solutions.” A key ‎part of this step is solutions being plural, meaning more than one. Why do designers and ‎engineers think of more than one way to solve a problem?‎

Objectives:‎

Students will obtain a greater understanding of how the engineering design processed is used to ‎solve real-world problems.‎

Teacher Instructions:‎

Adapt key phrases, concepts, and terms to best fit your students’ needs. Main idea is there is ‎NEVER any one solution to a problem. If possible, provide an example that relates to your ‎students’ lives, like all of their different shoes, or phones, or video game consoles. Emphasize ‎the importance of variety and why we must, as designers, think of as many ideas as possible.‎

Brainstorming Our Solutions

In this step of the engineering design process, students will begin to identify what type of ‎electronic circuit they wish to create. Specifications and constraints play a key role in design as ‎students identify what components and materials they have to work with.‎

During this stage, students may sketch what their final prototype will look like, as well as begin ‎to put together a bill of materials for what they need. Students should also consider and plan ‎their circuit’s schematics, or how components will be connected within the prototype in order ‎to ensure proper function and performance. Provide templates and resources for creating ‎schematic diagrams, such as planning documents or circuit design software.‎

Prior to fabricating final PCBs and prototype solutions, initial prototypes should be created ‎using simulation software, or prototyping tools such as breadboards as discussed in the first ‎step of this lesson. Removing any flaws in our designs now will lead to greater success later in ‎the engineering design process.‎

Teacher Instructions:‎

Emphasize coming up with as many ideas as possible as students will tend to want to go with ‎their first idea. Also reiterate the real-world specifications and constraints of the design ‎challenge and ensure students are factoring them into their designed solution. See the ‎‎“Modifications” and “Considerations” section of the lesson introduction for more examples on ‎how to modify this design challenge to cater to available resources.‎

Resources:

  • Design Challenge Brief Document [PDF]

  • Thumbnail Sketching Document [PDF]

  • Technical Drawing Paper [PDF]‎

Objectives:

  • Students will consider different possibilities as they brainstorm their prototype solutions

  • Students will plan and design a functioning electronic circuit with identified components

  • Students will prototype their circuit using physical components or simulation software

Exampleprint_5

‎Example 3D printed circuit board that combines analog components, ‎such as a pushbutton, resistor, battery,

and LED to make a simple light circuit ‎

Printed on a LulzBot Mini 2 with conductive and non-conductive PLA

Develop a Prototype

What is 3D Printing?‎

Step 3 of the engineering design process is all about constructing our prototype solution! In this ‎step, we are going to get hands-on with software and machinery to create our final designs.‎

One of the key prototyping machines used by today’s professional designers, engineers, and ‎scientists is a 3D printer. There are a lot of different types of 3D printers out there, but all 3D ‎printers create physical objects you can touch, and hold based on a 3D design or digital model. ‎Some 3D printers melt rolls of plastic into the model, while others use light to harden a liquid ‎resin. There are even 3D printers that can print concrete, metal, or living cell tissue!‎

LulzBot 3D printers use the fused deposition modeling process (FDM) that feeds and melts ‎spools of filament through a nozzle, kind of like glue traveling through a hot glue gun. The ‎plastic is fed, or extruded, layer by layer to create the model designed in computer aided ‎design (CAD) software. Some 3D printers, like the LulzBot TAZ Pro Dual Extruder, has more than ‎one nozzle and extruder to allow for multiple materials to be printed together!‎

When combining multiple types of filaments together, like rigid plastics with flexible ones, or ‎conductive materials with insulators, endless possibilities can be made! But you don’t ‎necessarily need a dual-extruder 3D printer to combine filaments, as discussed later in the ‎‎“Printing!” section of this lesson.‎

Objectives:‎

Students will be able to identify how 3D printers work, and how to use them safely.‎

Teacher Instructions:‎

Introducing and over viewing the resources available for prototyping before beginning ‎construction is key. Make sure your students know what resources are available, as well as how ‎to use them safely. Introduce any additional resources available for prototyping during this step ‎‎(see Modifications in lesson introduction.)‎

3dprinter_6

A LulzBot TAZ Pro with the Dual Extruder print head

creating a 3D printed PCB using both ‎conductive and non-

conductive PLA filament to create a prototype

Developing our 3D Models

Now that we’ve brainstormed our prototype PCB designs, it is time to begin to fabricate them! ‎But before we can 3D print our parts; we need a 3D design. To create this, we will use ‎computer aided design software, or CAD. There’s plenty of great free CAD programs out there, ‎we recommend Tinkercad, FreeCAD, Fusion360, or OnShape for students.‎

When creating 3D printed circuit boards, an added challenge arises as we need to design ‎conductive and insulation channels in our models to ensure functionality. To assist, we ‎recommend using PCB design software like KiCAD, Fritzing, or Fusion360 to create complex ‎multi-layer designs. Many CAD programs like Tinkercad allow you to import vector designs ‎from 2D design software. Combining applications may allow for students to create complex ‎paths with greater ease.‎

When creating models that work, we must also consider the properties of conductive filament. ‎Proto-Pasta’s conductive PLA has a greater conductivity across a single layer rather than ‎between multiple layers. This means that stronger electrical connections can be made with ‎models that are thin, rather than tall. When creating holes for components to fit into, shapes ‎that are too small will not be printed accurately. We recommend using 1/6” as a hole diameter ‎and dimension for creating tolerances. Note, model shrinking and required tolerances can vary ‎based on filament, printer, printing conditions, and print orientation.‎

Lastly, designs that will be manufactured on dual extruder printers may vary from ones that can ‎be produced on single extruder printers. Dual extrusion printers allow for materials to be ‎blended within layers, while single extrusion requires filament changes to occur from layer to ‎layer. Consider available resources when creating your 3D models - See more details about ‎layer changes in the next step.‎

Resources:

  • Computer or Tablet

  • USB Mouse (Recommended)

  • CAD Software & Guiding Tutorials

Objectives:‎

Students will utilize CAD Software to create a 3D model of their designed solutions. ‎

Teacher Instructions:‎

Students may better understand the purpose of CAD after being initially introduced to rapid ‎prototyping production machinery. For beginners, experimentation is key when learning the ‎basics of CAD software. Offer students guidelines for dimensions and tolerances as they begin ‎to create their designs in CAD (see Modifications in lesson introduction). Using specialized ‎software or 2D vector drawing programs may assist in creating PCB models that both function ‎and that can be accurately 3D printed.‎

Printhead_7

A LulzBot TAZ Pro with the Dual Extruder print head

creating a 3D printed PCB using both conductive and non-

conductive PLA filament to create a prototype

Printing

Once students have completed their designs, it’s time to download and prepare them to use ‎Cura LulzBot Edition. Cura is not a CAD program in that it allows you to design your models. Instead, Cura “slices” models layer by layer to create a program file, or Gcode file, for the 3D ‎printer to read. This Gcode file is a set of directions that the 3D printer follows as it prints your ‎model.

‎In general, we recommend PLA filament for most classroom uses as it’s a safe plastic to print in ‎schools and prints easily in nearly any setting. PLA works well for most applications and comes ‎in many variations that include varying color and properties. When creating our 3D printed ‎circuit boards, we will be combining two different types of PLA - conductive and non-conductive!

‎Dual extrusion 3D printers like the LulzBot TAZ Pro allow users to print two different types of ‎filaments at the within the same layer. This would allow you to merge two models together in ‎Cura LE to create a single part printed with two extruders and two different types of filaments. ‎Dual extrusion opens up new opportunities for prototyping as different filaments can be ‎combined within the same layer, allowing for infinite geometric freedom in your designs!‎

However, multi-material printing can be achieved with a single extruder 3D printer as well! ‎Instead of printing two materials within the same layer, a print can be paused at a specific ‎layer, then the filament can be changed. This will allow a user to begin a print with an insulator ‎filament, pause, then finish with a conductive filament to create a fully functional PCB! Using ‎Cura LE, you can modify your GCode to do this automatically. Using the Modify G-Code ‎extension under the Post Processing in the extensions menu, you can choose to pause at height ‎or layer in order to allow autonomous pausing for easy filament changes!‎

In addition to choosing the type of filament, we also must choose our printing detail, or layer ‎height. The smaller the layer height, the smoother and higher detail our models will be. In ‎general, printing at the high speed or standard detail setting will allow for student designs to be ‎printed quickly and at an effective quality for medium to large size models. We must also ‎consider our model density when printing with conductive filaments. A low infill density will ‎create a more hollow model which would be less conductive. Ideally, insulator parts can be ‎printed with a low density while conductor parts can be printed at a high density, or 100% infill. ‎This can be achieved easily by adjusting your print settings per extruder in Cura LulzBot Edition.‎

Objectives:‎

Students will understand how 3D models designed in CAD are prepared and sent to 3D printers ‎for manufacturing.‎

Teacher Instructions:‎

Depending on your student age group and classroom resources, the teacher may need to slice ‎the models for the students. Ensure proper settings are chosen for selected filament and model ‎quality. Reference LulzBot guides and tutorials for assistance.‎

Prepare_8

Preparing a prototype flashlight to be 3D printed on a LulzBot TAZ Pro Dual Extruder 3D printer in Cura LE

Modify_9

Modifying Gcode to pause at a specific layer for a filament change while preparing

a circuit board model to be printed on a LulzBot Mini 2 in Cura LE

You may also need to consider support material when printing models with overhangs or ‎potential structural flaws. Support material is automatically drawn by Cura and adds filament ‎structures that can be removed after printing. When printing with multiple types of filaments, ‎consider where supports will be placed before choosing which extruder (on dual extrusion ‎printers) will be printing the supports. For example, if supports need to be placed within a slot ‎for a battery that is made of conductive filament, the supports should also be conductive. This ‎will ensure no insulation material is placed or left where the model must be conductive. The ‎same goes for areas that must be insulated too. If you print supports with conductive material ‎that spans across insulated areas, accidental electrical connections might be made!‎

Discussing Gcode is a good lesson in itself! Gcode is a list of directions for the machines to ‎follow and can be read using a basic text program. When creating specialized post processing ‎modifications like pausing at a specific layer, an advanced used can manually edit the GCode ‎files to add these commands. Did you know early CNC machines required people to write Gcode ‎manually? Luckily, we have Cura for that now!‎

Creating_10

Creating a 3D printed circuit board using both non-conductive and conductive PLA filaments on a

single extruder LulzBot Mini 3D printer by pausing at a specific layer height to change filaments

Constructing our Prototypes

In the final part of this stage in the engineering design process, we must construct our ‎prototypes after all parts have been 3D printed. Depending on available resources and the ‎specifications and constraints of the challenge, this step may involve assembling 3D printed ‎parts together, installing electronic components in a simple design, or creating a complex PCB ‎one component at a time. Time will vary based on how many materials and resources students ‎have to build with.‎

To connect components to a 3D printed circuit board, a variety of methods can be used. Proper ‎fit and snap together install is ideal, or components can be secured using glue, conductive paste, ‎melting the filament around the connection, or even solder!‎

Remember, proper safety procedures should be introduced to students when working in any ‎makerspace or lab environment. When students are around machines such as 3D printers, or ‎using tools to cut or glue materials, students must be informed of potential hazards and taught ‎how to use these resources safely. For reference, see the safety resources offered by ITEEA.‎

Resources:‎

Materials and tools for prototype construction.

Objectives:‎

Students will use available resources and apply proper safety techniques to construct their prototype solutions.‎

Teacher Instructions:‎

Available resources and additional materials will vary based upon the specifications and ‎constraints of the design challenge. For examples, see the “Modifications” and “Considerations” ‎sections in the lesson introduction. Safety is key. Ensure all students have been trained to use ‎any available tools or resources and organize your room to ensure these resources can be ‎monitored accordingly.‎

assembly_11

‎Assembling conductive 3D printed parts onto a 3D printed ‎circuit board with an integrated potentiometer and switch ‎

Printed on a LulzBot Mini 2‎

Test and Evaluate

Testing Our Solutions

In this stage of the design process, it is time to get hands-on with our designed prototype ‎solutions in order to determine the effectiveness and success through testing!‎

Depending on the type of product or solution created, testing and evaluation steps may vary ‎from student to student. During this stage, students should record the successes and failures of ‎their prototype solution in order to obtain understandings of how well their prototypes perform. ‎Consider the following questions to guide evaluation:‎

  • Does the prototype function as intended?‎‎

  • Are all components secured properly?

  • What could be improved in terms of user interaction or prototype performance?‎‎

  • How does this printed circuit board and electronic prototype device compare to those of ‎industry or production quality?‎

Challenge students to work collaboratively as they test each other’s prototype solutions under ‎real-world specifications and constraints through the eyes of a creator and consumer. As each ‎prototype solution may differ in performance and function, guidelines for offering meaningful ‎and constructive feedback may be needed.‎

Resources:‎

Planning document or notebook to record findings and discoveries during testing stages of the ‎design process.‎

Objectives:‎

Students will apply the engineering design process as they test the performance of their ‎prototype solutions in a real-world setting.‎

Teacher Instructions:‎

Challenge students to think critically as they compare their designed solutions to the identified ‎problem at hand, as well as existing solutions. Remind students that these are PROTOTYPES, not ‎finished models and that failure or room for improvement is expected and GOOD when ‎designing solutions to real-world problems.‎

3dflashlight_12‎‎

3D printed flashlight prototype example with integrated circuit board and push button‎

Printed on a LulzBot TAZ Pro Dual Extruder combining both normal and conductive PLA ‎filaments

Redesign

No design is perfect, nor is it ever truly finished. As new technology is developed, improvements ‎like cost, speed, performance, or aesthetics can always be made. When considering redesign, ‎we must look at both the successes and failures of our prototypes. A failed design does not ‎mean we failed; it means we have room to improve upon for the next prototype solution.

‎Consider findings from testing and evaluating your 3D printed circuit board prototype solution, ‎as well the feedback obtained through sharing your solution with your peers as they tested it ‎under real-world constraints. What worked well? What could be improved? Create a sketch or ‎schematic diagram of an improved prototype design with changes you would make to allow ‎your prototype to better meet the evaluation criteria and solve our real-world problem. Your ‎sketch should be neat and label the changes you are making to improve your solution’s ‎performance.‎

Resources:‎

Planning document or Drawing Paper [PDF]‎

Objectives:‎

Students will utilize the engineering design process to reflect and improve upon their designs as ‎they create a proposed redesigned solution.‎

Teacher Instructions:‎

Stress the importance of failure in design and engineering. No one enjoys failing, or not doing ‎well, but the redesign step is a chance to reflect on both the good and bad of our designed ‎solutions. Additionally, we can use observations made from existing solutions and collaborating ‎with our peers as we create a proposed redesign with everything we’ve learned.

‎Drawn and written redesign activities both work well with varying learning styles, we ‎recommend a combination of the two. If time permits, students may use CAD to make a 3D ‎model of their redesigned solution or even attempt to create a new solution entirely.‎

sample_14

Sample layered light prototype example with an integrated circuit board

Printed on a LulzBot TAZ Pro Dual Extruder combining both normal and conductive PLA ‎filaments

מק"ט יצרן # RM-PL0100
FILAMENT BLACK PLA 0.112" 500G
LulzBot
מק"ט יצרן # KT-CP0162
LULZBOT TAZ DUAL EXTRUDER V3.1 T
LulzBot
₪ 1,677.16
הצגת עוד Details
מק"ט יצרן # RM-PL0206
3D-FUEL, STANDARD PLA, BRIGHTEST
LulzBot
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.