Maker.io main logo

4Duino Electronic Piano

22

2016-08-31 | By 4D Makers

License: None Arduino

 

When subjected to an alternating electric field, a piezo ceramic material disc inside the buzzer is caused to stretch or compress, in accordance with the frequency of the signal thereby producing sound. Buzzers are widely used in computers, alarms, toys, telephone and so on. For this project 4Duino resistive touch display is used as a means for a graphical user interface to play the piano.

How It Works

 Piano

Components

  • 4Duino
  • Active Buzzer
  • Jumper cables
  • Micro USB cable
  • µSD card

Implementation Step 1 : Build

Build the circuit as shown in the following diagram and schematic.

 schematic

Step 2: Program

Workshop 4 – 4Duino Extended Graphics environment is used to program this project.

This project requires the Arduino IDE to be installed as Workshop calls the Arduino IDE for compiling the Arduino sketches. The Arduino IDE however is not required to be opened or modified to program the 4Duino. 

Open this file using Workshop 4.

program

Step 3: Comms Port

Connect the 4Duino to the PC using µUSB cable.

Then navigate to the Comms tab and select the Comms port to which the 4Duino connected.

comms

Step 4 : Compile and Upload

Finally, go back to “Home” tab and now click on the “Comp’nLoad” button.

 comp

The Workshop 4 IDE will prompt you to insert a µSD card to the PC in order to save the widget images. Insert µSD card, select the appropriate drive and press button “OK”.

 copy

If the µSD card has the widget images you can click button “No Thanks”

Step 5 : Insert µSD card

After uploading the program in to the 4Duino, it will try to mount the µSD card. If the µSD card is not present it will prints an error message.

 pict

All you need to do is insert the µSD card you saved the image files to into the 4Duino.

Demonstration

Now you can play the electronic piano and have sound output from the buzzer.

demo1

demo2

Flow Chart – 4Duino Code

 fc

See more here.

מק"ט יצרן # 4DUINO-24
4DUINO ATMEGA32U4/ESP8266/PICASO
4D Systems Pty Ltd
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.