Maker.io main logo

Getting Started with Inky wHAT

56

2022-05-19 | By Pimoroni

License: See Original Project

Courtesy of Pimoroni

Guide by Pimoroni

This tutorial will show you how to install the Inky Python library, and then ‎walk through its functionality. You'll learn how to a couple of the fun Inky ‎wHAT examples, and how to display text and images.‎

‎(wHAT stands for wide-HAT, by the way)‎

You'll see that your Inky wHAT already has an image on it, straight out of the ‎box! This is because e-paper displays, like the one on Inky wHAT, allow you ‎to update them with an image and the image will persist even once you've ‎cut the power supply (i.e., switched off your Pi, or even removed the wHAT ‎altogether)! This means that you can use Inky wHAT as a swish conference ‎badge, completely powerlessly.‎

Inky wHAT comes completely assembled. If you're using it with a full-sized Pi, ‎like a Pi 3 B+, then you can use the included standoffs to mount everything ‎securely.‎

Installing the Software

Note that if you've previously installed the Inky pHAT Python library and ‎you're installing the Inky library they will live happily alongside each other, ‎so there's no need to get rid of the old library.‎

We always recommend using the most up-to-date version of Raspbian, as ‎this is what we test our boards and software against, and it often helps to ‎start with a completely fresh install of Raspbian, although this isn't necessary.‎

As with most of our boards, we've created a really quick and easy one-line-‎installer to get your Inky wHAT set up. We'd suggest that you use this ‎method to install the Inky wHAT software.‎

Open a new terminal, and type the following, making sure to type y or n when ‎prompted:‎

curl https://get.pimoroni.com/inky | bash

Once that's done, it’s probably a good idea to reboot your Pi to let the ‎changes propagate, if the installer doesn't prompt you to reboot.‎

Using the Software

Running the Built-in Examples

The Inky Python library comes with a handful of really beautiful examples. ‎The examples, that live in the /home/pi/Pimoroni/inky/examples folder, are divided ‎into universal ones that work with both the pHAT and wHAT in the topmost ‎folder, and then those that are specific to the pHAT or wHAT in ‎the phat and what folders respectively.‎

Let's look at how to run a wHAT-specific example first.‎

Assuming you used the one-line-installer to install the library, the examples ‎will have been downloaded to /home/pi/Pimoroni/inky/examples (if you cloned and ‎installed the library straight from GitHub then they will be in inky/examples). ‎Open a new terminal window, and type the following to navigate to the ‎examples folder:‎

cd /home/pi/Pimoroni/inky/examples/what‎

QUOTES EXAMPLE

The larger size of Inky wHAT means that you can fit quite a bit of text on it. ‎This quotes example uses Wikiquote and the wikiquotes Python library to ‎display quotes from some famous scientists and engineers who we admire.‎

In the terminal, type the following to run the example:‎

python3 quotes-what.py --colour "red"‎

Inky wHAT is only available in red/black/white for now, but if and when other ‎colours become available then you'll be able to change that colour to the ‎appropriate one.‎

It'll take a few seconds to find a quote and update it to the Inky wHAT display.‎

display_1

If you dig into the code (type nano quotes-what.py), you'll find the list of famous ‎people, and you can add or remove people as you wish (here's the list of ‎people on Wikiquote).‎

You'll also see a handy function called reflow_quote that's used to reflow the text ‎line by line to make sure it flows properly. As well as reflowing the text, the ‎code checks each quote to make sure that it fits on the Inky wHAT display.‎

NAME BADGE EXAMPLE

We'll look at how to run one of the universal examples on the wHAT now, the ‎name badge example. This example takes some command line arguments ‎that specify the type of display (wHAT, in this case) and colour of display that ‎you're using.‎

Command line arguments are extra pieces of information that you can pass ‎into programs straight from the command line.‎

Let's try the name badge example. It takes three arguments - --type, --colour, ‎and --name - the names of which should be fairly self-explanatory.‎

In the terminal, type the following:‎

python3 name-badge.py --type "phat" --colour "red" --name "Inigo Montoya"‎

‎(You can also use -t, -c, and -n)‎

It'll take a few seconds (around 15 usually) to update the whole display. e-‎paper displays work by pulling coloured particles up and down using different ‎voltages, so that's what all the pulsing of the display is (and why the image ‎persists).‎

For now, Inky wHAT is just available in red/black/white, but the code allows ‎for yellow/black/white and black/white displays if and when they become ‎available, by just changing the colour passed in via --colour.‎

And obviously change your name from "Inigo Montoya", unless that really is ‎your name?!‎

Like we said earlier, you can now completely detach your Inky wHAT and use ‎it as a completely powerless name badge, although it should be noted that ‎the image may fade gradually over the course of a day or so, but you can ‎easily perk it up again by reconnecting it to your Pi and running the script ‎again.‎

Building your Own Code

Let's take a look now at how to build your own code with Inky wHAT. ‎Because of the way that the new universal Inky library works now, there's ‎some boilerplate (yadda yadda code!) that we need at the top of any code ‎we're going to run.‎

In the terminal, type python3 to open a Python prompt.‎

Here's the boilerplate. Type it in line by line.‎

Copy Code
from inky import InkyWHAT

inky_display = InkyWHAT("red")
inky_display.set_border(inky_display.WHITE)

That code imports the InkyWHAT class from the inky library, creates an instance ‎of the class that we've called inky_display and to which we've passed the ‎argument "red" to tell it what colour our display is, and set the border colour ‎‎(the thin bit at the very edge of the display) to white.‎

Now we're ready to start displaying things on Inky wHAT!‎

Displaying Text on Inky wHAT

A common task that you might want to do is to display text on Inky pHAT. ‎You can use the Python Image Library (PIL) to display text, using regular ‎TrueType fonts. In fact, we'll be using PIL to display images and graphics on ‎Inky wHAT too.‎

We've made a Python fonts library to make it easy to use Open Font License ‎‎(OFL) fonts with our products that have displays. The ones that the Inky ‎library examples use will have be installed as part of the Inky library install.‎

You can also use fonts the regular way by downloading or transferring them ‎to your Pi and then using the path to the file.‎

We're going to display a simple "Hello, World!"" on Inky wHAT using the ‎Fredoka One font. Because the Inky wHAT display is nice and big, we'll make ‎our "Hello, World!" nice and big at 36 points, but you can experiment with ‎different sizes to get a feel for what works well on the display.‎

The Python Image Library (PIL) will have been installed when you ran the ‎installer, so there's no need to worry about installing it. Our boilerplate code ‎above has already set up what we need to write to the Inky wHAT display ‎itself, but we'll need to import and set up PIL now.‎

Type the following:‎

Copy Code
from PIL import Image, ImageFont, ImageDraw

img = Image.new("P", (inky_display.WIDTH, inky_display.HEIGHT))
draw = ImageDraw.Draw(img)

This imports three classes from PIL that we'll need, creates a new image, img, ‎that is the width and height of the Inky wHAT display, and then creates a ‎drawing canvas, draw, to which we can draw text and graphics.‎

Next, let's import the font we need, and create a variable called font that we ‎can use when we're writing text to the canvas.‎

Copy Code
from font_fredoka_one import FredokaOne

font = ImageFont.truetype(FredokaOne, 36)

If you want to use your own fonts, then simply replace FredokaOne above with ‎the path to your font file in quotes.‎

As we saw above, when we created the new image, there are ‎handy inky_display.WIDTH and inky_display.HEIGHT constants that tell us the width ‎and height of the Inky wHAT display, and we can get PIL to tell us the width ‎and height of our Hello, World! text, so that we can perfectly centre the text on ‎the display with a little bit of math!‎

Copy Code
message = "Hello, World!"
w, h = font.getsize(message)
x = (inky_display.WIDTH / 2) - (w / 2)
y = (inky_display.HEIGHT / 2) - (h / 2)

The x and y variables will tell the draw.text() function where to place the top left ‎corner of our text. We'll also have to tell the function what colour we want the ‎text (RED, BLACK, or WHITE), and pass it our font variable. Last of all, we'll set the ‎image with inky_display.set_image(img) and call the inky_display.show() function to tell ‎Inky wHAT to refresh the display with our text.‎

Copy Code
draw.text((x, y), message, inky_display.RED, font)
inky_display.set_image(img)
inky_display.show()

hello_2

Try experimenting with different text colours, fonts, and sizes!‎

Displaying Images on Inky wHAT

Displaying images on Inky wHAT requires a little bit of jiggery-pokery to ‎prepare your images properly. They should be PNG-8 images, 400x300 pixels, ‎and in indexed colour mode with a palette of just three colours - black, white, ‎and red - in exactly that order.‎

We'll run through how to prepare a simple image for Inky wHAT in the free ‎graphics package for Linux, GIMP.‎

First, in the terminal, we'll install GIMP by typing sudo apt install gimp and then ‎open it by typing gimp.‎

Go to the File menu and click New to create a new file. Make the image width ‎‎400 pixels and the image height 300 pixels.‎

Draw your picture. We went for a simple rectangle and circle in black and red.‎

Once you've finished drawing your picture, you'll need to change the colour ‎palette of the image to a three colour, indexed colour palette image, with the ‎colours in the order white, black, and red.‎

Go to the Image menu, then Mode, and select Indexed.‎

We've created an Inky colour palette that you can use. In the terminal, type git ‎clone https://github.com/pimoroni/inky to clone the GitHub repo. You'll find the colour ‎palette at inky/tools/inky-palette.gpl.‎

Select Use custom palette, then click the Palette selection dialogue button. Select Palette ‎file and then select the inky-palette.gpl palette file from the GitHub repo that we ‎just cloned.‎

The last thing to do is to export the image as a PNG. Go to the File menu and ‎then select Export as. Give your file a filename (we called ours inky.png) and save ‎it in your home directory, /home/pi. A dialogue box should pop up with the ‎options for saving it. Make sure that you check the Save background ‎colour checkbox, then click Export.‎

Now we have to display our image on Inky wHAT. If you haven't made an ‎image, you can try displaying the Inky pHAT logo file that's in the GitHub repo ‎at inky/examples/what/resources/InkywHAT-400x300.png.‎

In the terminal, type the following, remembering that you'll have to type the ‎boilerplate for the Inky library and PIL again if you left the Python prompt, and ‎replacing the filename with the name of your own image file if it's different to ‎ours:‎

Copy Code
img = Image.open("/home/pi/inky.png")
inky_display.set_image(img)
inky_display.show()

art_3

Your Inky wHAT should now be displaying your glorious art.‎

Let's take it a little further and see how to take something like a photo and ‎convert it to be displayed on Inky wHAT, all within PIL.‎

CONVERTING IMAGES TO BE DISPLAYED ON INKY WHAT

Here's what we'll do:‎

  1. Open the image
  2. Resize it to be 300 pixels tall
  3. Crop the image‎
  4. Convert the image to use the 3-colour palette used by Inky wHAT

We found a really nice geometric pattern that works really nicely with Inky ‎wHAT and this dithering method on Unsplash. It's below, if you want to use it, ‎or you can find it in the examples/what/resources/ folder, where it's called pattern-‎‎3.jpg.‎

pattern_4

In the terminal, type the following in your Python prompt to load in the image:‎

img = Image.open("pattern-3.jpg")‎

We're going to do some rejigging of it to resize, crop, resample, and recolour ‎it. First, we'll get the dimensions of the image we loaded and create some ‎variables that'll be the new sizes we want to resize to.‎

Copy Code
w, h = img.size

h_new = 300
w_new = int((float(w) / h) * h_new)
w_cropped = 400

The w_new and h_new are the width and height that we're going to resize the ‎image to. We use the aspect ratio of the original image to calculate the width. ‎Because this image is a bit wider than 4:3, we'll crop the width down to 400 ‎later.‎

Copy Code
img = img.resize((w_new, h_new), resample=Image.LANCZOS)

We're using Lanczos resampling which should give a really nice, resized ‎image.‎

Next, we're going to crop the image, so we have to work out the top left (x0, ‎y0) and bottom right (x1, y1) pixel coordinates that we'll crop to.‎

Copy Code
x0 = (w_new - w_cropped) / 2
x1 = x0 + w_cropped
y0 = 0
y1 = h_new

And now we can crop it!‎

Copy Code
img = img.crop((x0, y0, x1, y1))

The final thing we need to do is to convert the image from an RGB palette to ‎a white/black/red one that's compatible with Inky wHAT.‎

Copy Code
pal_img = Image.new("P", (1, 1))
pal_img.putpalette((255, 255, 255, 0, 0, 0, 255, 0, 0) + (0, 0, 0) * 252)

img = img.convert("RGB").quantize(palette=pal_img)

The two pal_img lines are creating the palette that we use for the conversion, ‎and the quantize method takes care of mapping the two palettes.‎

Finally, let's display the converted image on Inky wHAT!‎

Copy Code
inky_display.set_image(img)
inky_display.show()

downloaded_6 

You can find the whole example in the downloaded examples ‎in /home/pi/Pimoroni/inky/examples/what/ and run it as follows:‎

python3 dither-image-what.py --colour "red" --image "resources/pattern-3.jpg"‎

There are also a couple of other nice images from Unsplash in the resources ‎folder that work really well with Inky wHAT.‎

Taking it Further

The larger size of the display on Inky wHAT really opens up loads of ‎possibilities to do interesting things with it. There's plenty of space to show ‎lots of text, data, graphs, icons, you name it!‎

Here's a few ideas we thought of:‎

  • a detailed weather display with 5-day forecast
  • graphing sensor data from one of our BME680 environmental sensors
  • a to-do list
  • household chores rota
  • news headlines
  • a tiny, palm-sized e-reader, using Button SHIM as the controls

That's all folks!

מק"ט יצרן # PIM408
INKY WHAT BLACK/RED/WHITE EPD
Pimoroni Ltd
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.