Maker.io main logo

Minecraft Turbopad

146

2023-06-27 | By Adafruit Industries

License: None

Courtesy of Adafruit

Guide by John Park

Overview

 

Use the Macropad to send any command to Minecraft with just one ‎button press. Program twelve custom keys that can run commands ‎or key combos.‎

CircuitPython makes it simple to customize your Minecraft Turbopad ‎to run any command you like, even initiate latching mouse and key ‎combos, such as auto strip-mining mode.‎

Parts

‎-or-‎

CircuitPython

CircuitPython is a derivative of MicroPython designed to simplify ‎experimentation and education on low-cost microcontrollers. It ‎makes it easier than ever to get prototyping by requiring no upfront ‎desktop software downloads. Simply copy and edit files on ‎the CIRCUITPY drive to iterate.‎

CircuitPython Quickstart

Follow this step-by-step to quickly get CircuitPython running on your ‎board.‎

Download the latest version of CircuitPython for this board via ‎circuitpython.org

Click the link above to download the latest CircuitPython UF2 file.

Save it wherever is convenient for you.‎

save_1

button_2

The BOOT button is the button switch in the rotary encoder! To ‎engage the BOOT button, simply press down on the rotary encoder.‎

To enter the bootloader, hold down the BOOT/BOOTSEL ‎button (highlighted in red above), and while continuing to hold it ‎‎(don't let go!), press and release the reset button (highlighted in ‎blue above). Continue to hold the BOOT/BOOTSEL button until the ‎RPI-RP2 drive appears!‎

If the drive does not appear, release all the buttons, and then repeat ‎the process above.‎

You can also start with your board unplugged from USB, press, and ‎hold the BOOTSEL button (highlighted in red above), continue to ‎hold it while plugging it into USB, and wait for the drive to appear ‎before releasing the button.‎

A lot of people end up using charge-only USB cables and it is very ‎frustrating! Make sure you have a USB cable you know is good for ‎data sync.‎

You will see a new disk drive appear called RPI-RP2.‎‎ ‎

Drag the adafruit_circuitpython_etc.uf2 file to RPI-RP2.‎

drive_3

drive_4

The RPI-RP2 drive will disappear, and a new disk drive ‎called CIRCUITPY will appear.‎

That's it, you're done! :)‎

drive_5

Safe Mode

You want to edit your code.py or modify the files on ‎your CIRCUITPY drive but find that you can't. Perhaps your board ‎has gotten into a state where CIRCUITPY is read-only. You may have ‎turned off the CIRCUITPY drive altogether. Whatever the reason, safe ‎mode can help.‎

Safe mode in CircuitPython does not run any user code on startup ‎and disables auto-reload. This means a few things. First, safe ‎mode bypasses any code in boot.py (where you can ‎set CIRCUITPY read-only or turn it off completely). Second, it does ‎not run the code in code.py. And finally, it does not automatically ‎soft-reload when data is written to the CIRCUITPY drive.‎

Therefore, whatever you may have done to put your board in a non-‎interactive state, safe mode gives you the opportunity to correct it ‎without losing all of the data on the CIRCUITPY drive.‎

Entering Safe Mode

To enter safe mode when using CircuitPython, plug in your board or ‎hit reset (highlighted in red above). Immediately after the board ‎starts up or resets, it waits 1000ms. On some boards, the onboard ‎status LED (highlighted in green above) will blink yellow during that ‎time. If you press reset during that 1000ms, the board will start up in ‎safe mode. It can be difficult to react to the yellow LED, so you may ‎want to think of it simply as a slow double click of the reset button. ‎‎(Remember, a fast double click of reset enters the bootloader.)‎

In Safe Mode

If you successfully enter safe mode on CircuitPython, the LED will ‎intermittently blink yellow three times.‎

If you connect to the serial console, you'll find the following message.‎

Copy Code
Auto-reload is off.
Running in safe mode! Not running saved code.

CircuitPython is in safe mode because you pressed the reset button during boot. Press again to exit safe mode.

Press any key to enter the REPL. Use CTRL-D to reload.

You can now edit the contents of the CIRCUITPY drive. ‎Remember, your code will not run until you press the reset button, or ‎unplug and plug in your board, to get out of safe mode.‎

Flash Resetting UF2‎

If your board ever gets into a really weird state and doesn't even ‎show up as a disk drive when installing CircuitPython, try loading ‎this 'nuke' UF2 which will do a 'deep clean' on your Flash ‎Memory. You will lose all the files on the board, but at least you'll be ‎able to revive it! After loading this UF2, follow the steps above to re-‎install CircuitPython.‎

Download flash erasing "nuke" UF2‎

Macropad Assembly

 

The Macropad features hot-swap sockets for the switches -- gone are ‎the days of having to commit to one type of switch and solder it ‎down! Now, you can plug in your Cherry MX red keyswitches use ‎them for a while, get bored, decide it’s time to test out some lubed, ‎filmed, re-sprung Invyr Holy Pandas, and swap them just like that!‎

Switches into Plate

First, insert a couple pf keyswitches through the keyswitch plate. The ‎plate mechanically connects the switches to each other, which lends ‎some nice lateral stability to the keys.

key_6

key_7

Connect to Board

Carefully press the two switches into the switch sockets, being very ‎careful to align the legs so none bend!‎

connect_8

connect_9

Add Switches

Continue adding switches, being mindful of their orientation.‎

add_10

add_11

switcches_12

Backplate

You can add the optional backplate using four M3 x 6mm screws.‎

backplate_13

backplate_14

macro_14a

Keycaps

Now, you can add your keycaps! simply press them onto the ‎keyswitch stems until they are fully seated.‎

keycaps_15

keycaps_16

keycaps_17

Code and use the Minecraft ‎Turbopad

Text Editor

Adafruit recommends using the Mu editor for editing your ‎CircuitPython code. You can get more info in this guide.‎

Alternatively, you can use any text editor that saves simple text files.‎

Download the Project Bundle

Your project will use a specific set of CircuitPython libraries and ‎the code.py file, along with a folder full of key configuration files. To ‎get everything you need, click on the Download Project Bundle link ‎below, and uncompress the .zip file.‎

Drag the contents of the uncompressed bundle directory onto your ‎MACROPAD board's CIRCUITPY drive, replacing any existing files or ‎directories with the same names, and adding any new ones that are ‎necessary.‎

Download Project Bundle‎

Copy Code
# SPDX-FileCopyrightText: 2021 John Park for Adafruit Industries
# SPDX-License-Identifier: MIT
# Minecraft Turbopad for Adafruit Macropad RP2040
import time
import displayio
import terminalio
from adafruit_display_text import bitmap_label as label
from adafruit_displayio_layout.layouts.grid_layout import GridLayout
from adafruit_macropad import MacroPad

macropad = MacroPad()

# --- Variable setup for action types
KEEB = 0
MEDIA = 1
MOUSE = 2
KBMOUSE = 3
COMMAND = 4

KEY_MOMENT = 0 # momentary press/release keys
KEY_HOLD = 1 # toggle keys

# --- LED colors
GREEN = 0x00ff00
RED = 0xff0000
MAGENTA = 0xff0033
YELLOW = 0xffdd00
AQUA = 0x00ffff
LATCH_COLOR = YELLOW
# --- Key mappings
# (<key>): (<color>, <action type>, <key hold>, <keycodes>, <"text">, <enter>)
keymap = {
(0): (AQUA, COMMAND, KEY_MOMENT, [macropad.Keycode.FORWARD_SLASH],
"gamemode creative", [macropad.Keycode.ENTER]),
(1): (AQUA, COMMAND, KEY_MOMENT, [macropad.Keycode.FORWARD_SLASH],
"gamemode survival", [macropad.Keycode.ENTER]),
(2): (AQUA, COMMAND, KEY_MOMENT, [macropad.Keycode.FORWARD_SLASH],
"say Dinner Time!", [macropad.Keycode.ENTER]),

(3): (AQUA, COMMAND, KEY_MOMENT, [macropad.Keycode.FORWARD_SLASH],
"time set day", [macropad.Keycode.ENTER]),
(4): (AQUA, COMMAND, KEY_MOMENT, [macropad.Keycode.FORWARD_SLASH],
"time set night", [macropad.Keycode.ENTER]),
(5): (AQUA, COMMAND, KEY_MOMENT, [macropad.Keycode.FORWARD_SLASH],
"kill", [macropad.Keycode.ENTER]),

(6): (GREEN, COMMAND, KEY_MOMENT, [macropad.Keycode.FORWARD_SLASH],
"weather clear", [macropad.Keycode.ENTER]),
(7): (GREEN, COMMAND, KEY_MOMENT, [macropad.Keycode.FORWARD_SLASH],
"weather rain", [macropad.Keycode.ENTER]),
(8): (GREEN, COMMAND, KEY_MOMENT, [macropad.Keycode.FORWARD_SLASH],
"weather thunder", [macropad.Keycode.ENTER]),

(9): (RED, COMMAND, KEY_MOMENT, [macropad.Keycode.FORWARD_SLASH],
"summon minecraft:bee", [macropad.Keycode.ENTER]),
(10): (RED, KBMOUSE, KEY_HOLD, [macropad.Keycode.W], [macropad.Mouse.LEFT_BUTTON]),
(11): (RED, COMMAND, KEY_MOMENT, [macropad.Keycode.FORWARD_SLASH],
"playsound minecraft:block.bell.use ambient @a ~ ~ ~", [macropad.Keycode.ENTER]),
}


latched = [False] * 12 # list of the latched states, all off to start

last_knob_pos = macropad.encoder # store knob position state

# --- Pixel setup --- #
macropad.pixels.brightness = 0.1
for i in range(12):
macropad.pixels[i] = (keymap[i][0])


main_group = displayio.Group()
macropad.display.show(main_group)
title = label.Label(
y=4,
font=terminalio.FONT,
color=0x0,
text=" -Minecraft Turbopad- ",
background_color=0xFFFFFF,
)
layout = GridLayout(x=0, y=13, width=128, height=54, grid_size=(3, 4), cell_padding=5)
label_text = [
"CREATE", "SURVIV", "SAY",
"DAY", "NIGHT", "KILL",
"CLEAR", "RAIN", "THUNDR",
"BEE", "MINE", "SOUND",
]
labels = []
for j in range(12):
labels.append(label.Label(terminalio.FONT, text=label_text[j]))

for index in range(12):
x = index % 3
y = index // 3
layout.add_content(labels[index], grid_position=(x, y), cell_size=(1, 1))

main_group.append(title)
main_group.append(layout)

while True:
key_event = macropad.keys.events.get() # check for key press or release
if key_event:
if key_event.pressed:
key = key_event.key_number
labels[key].color = 0x0
labels[key].background_color = 0xffffff

if keymap[key][1] == KEEB:
if keymap[key][2] == KEY_HOLD:
macropad.keyboard.press(*keymap[key][3]) # * expands the variable to list
else:
macropad.keyboard.send(*keymap[key][3])

elif keymap[key][1] == MOUSE:
macropad.mouse.click(*keymap[key][3])

elif keymap[key][1] == KBMOUSE:
if keymap[key][2] == KEY_HOLD:
if latched[key] is False:
macropad.keyboard.press(*keymap[key][3])
time.sleep(0.01)
macropad.mouse.press(*keymap[key][4])
latched[key] = True
else:
macropad.keyboard.release(*keymap[key][3])
time.sleep(0.01)
macropad.mouse.release_all()
latched[key] = False

elif keymap[key][1] == COMMAND:
macropad.keyboard.send(*keymap[key][3])
time.sleep(0.1)
macropad.keyboard_layout.write(keymap[key][4])
time.sleep(0.1)
macropad.keyboard.send(*keymap[key][5])
time.sleep(0.1)
macropad.pixels[key] = LATCH_COLOR

if key_event.released:
key = key_event.key_number
if keymap[key][1] == KEEB:
if keymap[key][2] == KEY_HOLD:
macropad.keyboard.release(*keymap[key][3])

if latched[key] is False:
macropad.pixels[key] = (keymap[key][0])
labels[key].color = 0xffffff
labels[key].background_color = 0x0

current_knob_position = macropad.encoder

if macropad.encoder > last_knob_pos:
macropad.mouse.move(wheel=-1)
last_knob_pos = current_knob_position

if macropad.encoder < last_knob_pos:
macropad.mouse.move(wheel=+1)
last_knob_pos = current_knob_position

View on GitHub

Use It

The Minecraft Turbopad acts just like a regular USB keyboard, so you ‎don't need to do anything tricky to enable it -- in fact, just fire up ‎Minecraft and start using it once you're playing! Press a key and the ‎command will run, just like that!‎

Here's a video of it in action:‎

Customize the Commands

You can switch out the commands to any that you prefer! Here's a ‎pretty comprehensive list for reference.‎

The keymap dictionary contains all of the commands, per key. For ‎example:‎

‎(0): (AQUA, COMMAND, KEY_MOMENT,

[macropad.Keycode.FORWARD_SLASH],

             ‎ "gamemode creative", [macropad.Keycode.ENTER])‎

That is the first entry, so it triggered by the first (upper left) key on ‎the Macropad. When pressed it will type out /gamemode creative. If you ‎wanted to change this to switch you into adventure mode, the line ‎would look like this:‎

‎(0): (AQUA, COMMAND, KEY_MOMENT,

[macropad.Keycode.FORWARD_SLASH],

           ‎ "gamemode adventure", [macropad.Keycode.ENTER])‎

Display Labels

When you customize your key commands, you'll want to update the ‎display labels to match. This code is the list you'll need to change, ‎simply swap in different text -- just keep it short and sweet so it fits ‎on screen!‎

Download File‎

Copy Code
label_text = [
"CREATE", "SURVIV", "SAY",
"DAY", "NIGHT", "KILL",
"CLEAR", "RAIN", "THUNDR",
"BEE", "MINE", "SOUND",
]
מק"ט יצרן # 5103
MACROPAD RP2040 HARDWARE KIT
Adafruit Industries LLC
מק"ט יצרן # 5122
KAILH MECHANICAL KEY SWITCHES -
Adafruit Industries LLC
מק"ט יצרן # 5068
CLEAR KEYCAPS FOR MX COMPATIBLE
Adafruit Industries LLC
מק"ט יצרן # 5153
CABLE A PLUG TO C PLUG 3.28'
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.