Maker.io main logo

Intro to ROS Part 8: Using Parameters to Configure ROS 2 Nodes

213

2025-11-13 | By ShawnHymel

Single Board Computers Raspberry Pi SBC

One of the key strengths of ROS 2 is its flexibility. So far in our tutorials, we've built publisher and service nodes with hardcoded values, such as the message to publish or the delay between timer callbacks. While this is fine for simple prototypes, it quickly becomes limiting in real-world applications. Fortunately, ROS 2 offers a better way: parameters.

In this tutorial, we'll explore how to use parameters in ROS 2 to dynamically configure nodes. You'll learn how to set parameters at runtime, update them while a node is running, and make your nodes more reusable and adaptable. We'll implement examples in both Python and C++ using a basic publisher node that emits a message to a topic.

The Docker image and code for this series can be found here: https://github.com/ShawnHymel/introduction-to-ros

Why Parameters Matter

Parameters allow you to define and update configuration values without modifying your source code. For example, you can reuse the same node to publish different messages or at different rates by simply changing parameters. This is incredibly useful for tuning robots or adapting behaviors without needing to recompile or redeploy your software.

Parameters are defined and accessed using the rclpy and rclcpp libraries in Python and C++, respectively. When a node launches, you can specify parameters using command-line arguments or configuration files. You can also update certain parameters while the node is running, which makes them even more powerful.

Basic Parameter Use in Python

Let’s start by modifying the minimal publisher example in Python. We'll create a new file called publisher_with_params.py and define two parameters: message and timer_period. The message parameter sets what string will be published, and timer_period sets the interval between publications.

Copy Code
import rclpy
from rclpy.executors import ExternalShutdownException
from rclpy.node import Node
from example_interfaces.msg import String
class PublisherWithParams(Node):
    """Publisher example that periodically sends out a string"""

    def __init__(self):
        """Constructor"""

        # Call the Node class constructor with the node name
        super().__init__('publisher_with_params')

        # Declare parameters
        self.declare_parameter('message', "Hello")
        self.declare_parameter('timer_period', 1.0)

        # Set to attributes
        self._message = self.get_parameter('message').value
        self._timer_period = self.get_parameter('timer_period').value

        # Create a publisher object
        self._publisher = self.create_publisher(String, 'my_topic', 10)

        # Periodically call method
        self._timer = self.create_timer(
            self._timer_period, 
            self._timer_callback
        )

    def _timer_callback(self):
        """Publishes a simple message to topic"""

        # Fill out String message
        msg = String()
        msg.data = self._message

        # Publish message to topic
        self._publisher.publish(msg)
        self.get_logger().info(f"Publishing: {msg.data}")

def main(args=None):
    """Main entrypoint"""

    # Initialize and run node
    try:
        rclpy.init()
        node = PublisherWithParams()
        rclpy.spin(node)

    # Catch ctrl+c or shutdown request
    except (KeyboardInterrupt, ExternalShutdownException):
        pass

    # Destroy node (now) and gracefully exit
    finally:
        if node is not None:
            node.destroy_node()
        if rclpy.ok():
            rclpy.shutdown()

if __name__ == '__main__':
    main()

Add the following executable to setup.py:

Copy Code
"publisher_with_params = my_py_pkg.publisher_with_params:main",

Build the package:

Copy Code
colcon build --packages-select my_py_pkg

When you run the node with no arguments, it uses the default parameters. But you can override them at runtime like this:

source install/setup.bash
ros2 run my_py_pkg publisher_with_params --ros-args -p message:="Hi from ROS2!" -p timer_period:=0.5

These values are only set at startup. If you stop and restart the node, it resets to the defaults unless you specify the parameters again.

You can echo the messages in another terminal:

Copy Code
ros2 topic echo /my_topic

Image of Intro to ROS Part 8: Using Parameters to Configure ROS 2 Nodes

Updating Parameters at Runtime (Python)

To support dynamic updates to parameters while the node is running, we can use the add_post_set_parameters_callback() method. This allows us to respond when a parameter is changed. Modify the self.__init__() method and add a self.add_post_set_parameters_callback() method to your node:

Copy Code
import rclpy
from rclpy.executors import ExternalShutdownException
from rclpy.node import Node
from example_interfaces.msg import String

class PublisherWithParams(Node):
    """Publisher example that periodically sends out a string"""

    def __init__(self):
        """Constructor"""

        # Call the Node class constructor with the node name
        super().__init__('publisher_with_params')

        # Declare parameters
        self.declare_parameter('message', "Hello")
        self.declare_parameter('timer_period', 1.0)

        # Set to attributes
        self._message = self.get_parameter('message').value
        self._timer_period = self.get_parameter('timer_period').value

        # Configure callback for runtime parameter update
        self.add_post_set_parameters_callback(self._post_parameters_callback)

        # Create a publisher object
        self._publisher = self.create_publisher(String, 'my_topic', 10)

        # Periodically call method
        self._timer = self.create_timer(
            self._timer_period, 
            self._timer_callback
        )

    def _timer_callback(self):
        """Publishes a simple message to topic"""

        # Fill out String message
        msg = String()
        msg.data = self._message

        # Publish message to topic
        self._publisher.publish(msg)
        self.get_logger().info(f"Publishing: {msg.data}")

    def _post_parameters_callback(self, params):
        """Set parameter after node started"""

        # Loop through all parameters
        for param in params:

            # Update message
            if param.name == 'message':
                self._message = param.value
                self.get_logger().info(f"Set {param.name} to {param.value}")

            # Update timer
            elif param.name == 'timer_period':

                # Update member variable
                self._timer_period = param.value
                self.get_logger().info(f"Set {param.name} to {param.value}")

                # Reset timer
                self._timer.cancel()
                self._timer = self.create_timer(
                    self._timer_period,
                    self._timer_callback
                )

            # Unknown parameter
            else:
                self.get_logger().warn(f"Unknown parameter: {param.name}")

def main(args=None):
    """Main entrypoint"""

    # Initialize and run node
    try:
        rclpy.init()
        node = PublisherWithParams()
        rclpy.spin(node)

    # Catch ctrl+c or shutdown request
    except (KeyboardInterrupt, ExternalShutdownException):
        pass

    # Destroy node (now) and gracefully exit
    finally:
        if node is not None:
            node.destroy_node()
        if rclpy.ok():
            rclpy.shutdown()

if __name__ == '__main__':
    main()

Build the package again:

Copy Code
colcon build --packages-select my_py_pkg

In one terminal, run the publisher:

Copy Code
source install/setup.bash
ros2 run my_py_pkg publisher_with_params --ros-args -p message:="Hi from ROS2!"

In a second terminal, echo the messages:

Copy Code
ros2 topic echo /my_topic

In a third terminal, dynamically update the parameters to the publisher:

Copy Code
ros2 param list
ros2 param set /publisher_with_params message "Greetings."
ros2 param set /publisher_with_params timer_period 0.5

You should see the message text and frequency change.

Image of Intro to ROS Part 8: Using Parameters to Configure ROS 2 Nodes

Using Parameters in C++

Let’s port the same example to C++. Start with a copy of your minimal_publisher.cpp, and update it to declare, retrieve, and monitor parameters.

Copy Code
#include "rclcpp/rclcpp.hpp"
#include "example_interfaces/msg/string.hpp"

/**
 * Publisher example that periodically sends out a string
 */
class PublisherWithParams : public rclcpp::Node
{

public:

Copy Code
 /**
   * Constructor (call Node class constructor with node name)
   */
  PublisherWithParams() : Node("publisher_with_params")
  {
    // Declare parameters
    this->declare_parameter("message", "Hello");
    this->declare_parameter("timer_period", 1.0);

    // Get parameters and set to member variables
    message_ = this->get_parameter("message").as_string();
    timer_period_ = this->get_parameter("timer_period").as_double();

    // Configure callback for runtime parameter update
    param_cb_handle_ = this->add_post_set_parameters_callback(
      std::bind(
        &PublisherWithParams::post_parameters_callback,
        this,
        std::placeholders::_1));

    // Create a publisher object
    publisher_ = this->create_publisher<example_interfaces::msg::String>(
      "my_topic",
      10);

    // Periodically call method
    timer_ = this->create_wall_timer(
      std::chrono::milliseconds(500),
      std::bind(&PublisherWithParams::timer_callback, this));
  }

private:

Copy Code
/**
   * Publishes simple message to topic
   */
  void timer_callback()
  {
    // Fill out String message
    auto msg = example_interfaces::msg::String();
    msg.data = message_;

    // Publish message to topic
    publisher_->publish(msg);
    RCLCPP_INFO(this->get_logger(), "Publishing: %s", msg.data.c_str());
  }

  /**
   * Set parameter after node started
   */
  void post_parameters_callback(
    const std::vector<rclcpp::Parameter> &parameters)
  {
    // Loop through all parameters
    for (const auto &param : parameters) {

      // Update message
      if (param.get_name() == "message") {
        message_ = param.as_string();
        RCLCPP_INFO(
          this->get_logger(),
          "Set %s to %s",
          param.get_name().c_str(),
          param.as_string().c_str());
      }

      // Update timer period
      else if (param.get_name() == "timer_period") {

        // Update member variable
        timer_period_ = param.as_double();
        RCLCPP_INFO(
          this->get_logger(),
          "Set %s to %f",
          param.get_name().c_str(),
          param.as_double());
      
        // Reset timer
        timer_->cancel();
        timer_ = this->create_wall_timer(
          std::chrono::duration<double>(timer_period_),
          std::bind(&PublisherWithParams::timer_callback, this));
      }

      // Unknown parameter
      else {
        RCLCPP_WARN(
          this->get_logger(),          
        "Unknown parameter: %s",
          param.get_name().c_str());
      }
    }
  }

  // Declare member variables
  std::string message_;
  double timer_period_;
  rclcpp::Publisher<example_interfaces::msg::String>::SharedPtr publisher_;
  rclcpp::TimerBase::SharedPtr timer_;
  rclcpp::node_interfaces::PostSetParametersCallbackHandle::SharedPtr
    param_cb_handle_;
};

/**
 * Main entrypoint
 */
int main(int argc, char * argv[])
{
  // Initialize ROS 2
  rclcpp::init(argc, argv);

  // Initialize and run node
  auto node = std::make_shared<PublisherWithParams>();
  rclcpp::spin(node);

  // Cleanup
  rclcpp::shutdown();

  return 0;
}

Add the executable to CMakeLists.txt

Copy Code
# Define trigger_points_client target and link libraries
add_executable(publisher_with_params src/publisher_with_params.cpp)
ament_target_dependencies(publisher_with_params rclcpp example_interfaces)

# Install binaries to specific folder
install(TARGETS
 minimal_publisher
 minimal_subscriber
 minimal_server
 minimal_client
 acc_subscriber
 trigger_points_client
 publisher_with_params
 DESTINATION lib/${PROJECT_NAME})

Build the package:

Copy Code
colcon build --packages-select my_cpp_pkg

In one terminal, run:

Copy Code
source install/setup.bash
ros2 run my_cpp_pkg publisher_with_params --ros-args -p message:="Hi from ROS2!"

In a second terminal:

Copy Code
ros2 topic echo /my_topic

In a third terminal:

Copy Code
ros2 param set /publisher_with_params message "Greetings."
ros2 param set /publisher_with_params timer_period 0.5

Just like with the Python example, you should see the message and frequency change.

Image of Intro to ROS Part 8: Using Parameters to Configure ROS 2 Nodes

Summary

In this tutorial, we explored how to use parameters in ROS 2 to make your nodes more flexible and configurable. We learned how to declare parameters, read them at startup, and update them at runtime using both Python and C++. Parameters are a key part of writing robust and reusable ROS 2 applications, especially in scenarios where tuning and runtime adaptability are critical.

By using parameters, you eliminate the need for recompilation or editing source code just to change configuration values. This leads to cleaner, more maintainable codebases and a smoother development workflow. As your projects grow in complexity, the ability to dynamically configure nodes becomes increasingly important. In the next part of the series, we'll look at launch files and how to orchestrate complex systems using parameterized configurations.

Stay tuned!

מק"ט יצרן # 28009
EXPERIENTIAL ROBOTICS PLATFORM (
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.