Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
revolution
3M brand Round Conductor Flat, Controlled Impedance Cable, 7700 Series is a 0.025" pitch flat ribbon cable that can support up to 14 Gbps when terminated to an IDC connector – or up to 20 Gbps when using the cable only. The performance of the 7700 Series is made possible because of a revolutionary construction that not only enables outstanding throughput, but also accommodates tighter folding than conventional jacketed shielded cables – and with minimal performance impact. It is constructed using 30 AWG solid copper conductors in polyolefin insulation. The outer insulation is a laminated, flexible foil covering which controls the impedance at 95 ohms (±5 ohms). It does not, however, act as an EMI/RFI shield. The cable can be terminated to .050" spaced IDC connectors, such as the 451 and 820 Series, as well as Mini Delta Ribbon System, also from 3M. If properly prepped, the cable may be directly attached by solder to traces on a PCB. 3M offers the cable in conductor counts in increments of 10 through 100.
PTM פורסם ב: