Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
Image of Advantech ADAM-6717SK Intelligent I/O Gateway Starter Kit - Facility Monitoring

With the starter kit, users can simulate scenarios in facility monitoring. The analog input on the ADAM-6717 will acquire sensor signals such as temperature and gas. When values go out of specification the gateway can trigger the digital outputs such as the buzzer and fan for alarms. The crash sensor and button are connected to the digital outputs of the ADAM-6717 to monitor the status. All the values are visualized with the node-red dashboard.

PTM פורסם ב: