Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Basics of Wire and Cable Slide 13

The temperatures at which a cable can function effectively are, in part, determined by the insulation. The temperature rating of the insulation is the range of temperatures at which material can be used without degradation. In the technical information section of the Alpha Wire catalog, various ratings for all of the insulation materials used are listed.

PTM פורסם ב: