Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
HotSwap-Slide10

The MOSFET is the most critical part of the hot swap control circuit. This is the main switch which, if damaged, could result in the board not powering up or never powering down. Selection begins by determining the maximum operating current, multiplying this by 2, and looking for current ratings higher than the result. This elevated rating will protect against surges and transients that may damage the MOSFET. In high current systems, the RDSon is very important in that the lower the better since high “on” resistances will result in voltage drops and power loss. To determine the maximum voltage required, use the same approach as when determining the current in that the rated Vds of the MOSFET should be greater than 2x the nominal voltage to protect against transients.

PTM פורסם ב: