Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
HotSwap-Slide15

Ideally this MOSFET can survive this power combination for a maximum of 8ms. However, due to tolerances and other variations, it is advisable to design in a margin of error. Therefore, a value lower than this should be selected, somewhere between 1 to 5ms for example. Once this time is obtained, the TIMER capacitor is calculated as shown.

PTM פורסם ב: