Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
HotSwap-Slide6

Internally the controller has the following main blocks: 1) A current sense amplifier which senses the voltage drop across the sense resistor and gains it up to provide a more practical voltage, 2) An over-current comparator which tells the controller when the current limit is reached, 3) A TIMER circuit which injects a current into an external capacitor which is used to time a cycle once the current limit is reached. When this time expires the MOSFET is disabled, and 4) A gate drive charge pump circuit which enhances the GATE voltage to a level that is sufficiently higher than Vcc in order to fully enhance the Gate of an N-Channel MOSFET.

PTM פורסם ב: