Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
HotSwap-Slide28

The second commonly used architecture is the low voltage positive area. An example of this is a 12V storage system where the main power switch is on the high side with the hot swap controller residing there also. The ADM1177 is shown in this configuration. In this case, the gate voltage needs to be higher than the main supply to enhance the N-channel MOSFET. The ADM1177 also integrates digital power monitoring to allow the user to digitally read back the voltage and the current.

PTM פורסם ב: