Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
HotSwap-Slide20

If multiple MOSFETs are required to dissipate the total power, then care must be taken not to assume the load will be shared evenly. During normal operation the load will most likely be shared across all MOSFETs. However, on power up the load may be shared unevenly due to the slightly differing Vgsth of the MOSFETs. This is why each MOSFET must be capable of tolerating the maximum load individually. When the MOSFET is a surface mount component, is may be desirable to transfer some of the heat from the MOSFET to a metal area on the other side of the PCB. This can be done with a via array which will provide a thermally conductive path through the PCB to the other side. This however will not be very efficient.

PTM פורסם ב: