Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
HotSwap-Slide11

Another factor to be aware of is the Vgsth of the MOSFET which indicates if the controller can adequately drive the gate to full enhancement. Having the proper Vgsth will ensure minimum power loss across the MOSFET and lowest heat dissipation. Finally, the Safe Operating Area (SOA) must be maintained in order to protect the MOSFET from destruction. The TIMER capacitor, discussed next, will ensure the SOA is maintained. The load capacitance will have a factor in determining the length of time it may take for the load voltage to rise up. The SOA should therefore be long enough to complete this in charge-up conditions and yet short enough at worst case conditions to protect the MOSFET.

PTM פורסם ב: