Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
HotSwap-Slide24

During a short circuit event, the current will attempt to increase to the maximum available from the supply. The controller will respond as follows: 1) The output voltage is pulled to GND, 2) The load current will then surge towards the maximum allowed by line impedance and inductance, 3) Once the current has exceeded the limit, the controller responds by pulling down the gate voltage to the MOSFET, shutting it down, 4) When the current is below the threshold the gate will begin to rise again and will hold the current at the limit until the TIMER expires. Then it will shut down the MOSFET.

PTM פורסם ב: