Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
HotSwap-Slide21

Inrush Current can be substantial when dealing with high current systems using large hold-up capacitors which may require hundreds or thousands of Amps if left uncontrolled. The hot swap controller limits the current at a preset limit, however, there is still an immediate inrush of current (from 0 to 10A or higher) to charge the capacitors up to this limit. In the cases where the nominal limit is high, this can be a problem as this will cause unwanted transients. The Soft Start function will slowly ramp this current limit from ~20% to 100% of the current limit at a rate determined by the Soft Start Capacitor.  The larger the capacitor the slower the inrush current ramp profile.

PTM פורסם ב: