Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Differential-Circuit-Slide10

Taking the same mathematical approach to look at the differential approach there can be seen an inherent cancellation of even-order harmonics, a benefit similar to the previously discussed common mode interference immunity. Again, a non-linear device, in this case a differential amplifier block, is described by a power-series expansion transfer function and is supplied with a pair of sinusoids of opposite polarities – these represent a differential signal at the device’s inputs. Through expansion, the cancellation effect of the differential block is shown.

PTM פורסם ב: