Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
ATmega128RFA1-Slide8
Keeping active current consumption to the minimum is also an important factor when designing battery-operated wireless systems. The Microchip ATmega128RFA1 offers unmatched power consumption figures for the AVR microcontroller in active mode of 0.26mA/MHz. This gives a maximum current consumption of 4.1mA running the AVR at a maximum speed of 16MHz.
PTM פורסם ב: