Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
XMEGA-USB-Connectivity-Slide4

A small experiment was created to compare the data rates achieved using normal and ping-pong buffering. An XMEGA was set to transfer data using USB in BULK transfer mode. This mode has a maximum packet size of 64 bytes. As one can see in the table, the benefits of the ping-pong mode are obvious. The bandwidth has increased significantly to 8.7 Mb/s, boosting the performance of the application and closing in on the theoretical maximum data rate. 

PTM פורסם ב: