Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
zigbee-lowpower-Slide13

The ZigBee standard allows the following binding types: one-to-one, a single sensor is bound to the central node; many-to-one, several sensors of the same type are bound to the same central node; and one-to-many, a single switch is used to control several nodes simultaneously.

PTM פורסם ב: