Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
PowerProtector and AutoRefresh Technologies Slide 8

When writing data onto Flash chips, the data is divided into segments of mini-second (ms)-long program operations. These subdivided operations are written onto the Flash chips one operation at a time. The Figure here illustrates an example of a blackout occurring during multiple segments of mini-second (ms)-long program operations. A device without advanced power protection technology such as ATP’s PowerProtector can only provide limited data protection and may lose the data in the 8th mini-second-long programming operation. The data, written by the previous program operation 7 and prior operations is retained, as the data has already been written onto the Flash chips during programming operations 1 to 7. However, after a reboot, if the host tries to access the data written by program operation 8, a data error will occur.

PTM פורסם ב: