Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Product List
TurboCap-Slide3

Expanding on the three initial values, AVX added twelve new values and continues to develop others to meet market needs. As can be seen in the image on this page, this is a very small device. Their small size coupled with capacitance values of 220μf @ 25V or 47μf @ 100V makes this a very useful part for applications such as high-end DC/DC converters, general power supplies, telecom networks, snubbers and more. In some cases, several components (such as AL-EL, tantalum or other devices) can be replaced with a smaller TurboCap™ and achieve better performance and a smaller overall footprint.

PTM פורסם ב: