Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
1000v
At 1000 VDC, conduction losses are the primary source of heating versus switching losses. Regardless, under these conditions the Wolfspeed SiC MOSFET is still operating at 15-20o lower than the silicon MOSFET. As before, under these operating parameters, the Wolfspeed device can safely operate without a heatsink. At 80˚C, it is only running at roughly 1/2 of the maximum junction temperature.
PTM פורסם ב: