Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
FX3 USB 3 Solution Slide 10

The third step is to develop a prototype quickly using the HD 720p camera kit. First, connect the Aptina image sensor headboard to the FX3 DVK in two steps: one, attach the interconnect board to the GPIF II connector of the FX3 DVK; next attach the Aptina image sensor headboard to the interconnect board. Once the setup is complete, connect the FX3 DVK to a PC via USB 3.0 cable and install the Cypress USB 3.0 driver. Program the FX3 DVK with image sensor firmware using the Cypress control center. The FX3 DVK will connect to the PC automatically as a UVC camera. At this time the designer can run AMCap or equivalent software on the PC to view live HD 720p video.

PTM פורסם ב: