Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
Slide3
Mass consumer uses of proximity aware devices are called ‘beacons’ and ‘tags’. The SmartBond DA1458 series of devices are a breakthrough solution for applications which require very small batteries while requiring long lifetimes. Neither application can use rechargeable power sources and are cost sensitive. Battery life, size and system cost are all important and the DA1458 series provides one of the best in class performances in these areas
PTM פורסם ב: