Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
Chat Session via XBee Slide 14

If it is not already there, add an XBee to XCTU so it is listed in the Radio Modules list. If using two computers, add the module attached to one of the PCs to the corresponding instance of XCTU. Open the serial connection of the radio module: select the XBee in the Radio Modules section, and click the Open serial connection button. Note: the background will change to green to indicate that the connection is open. Repeat steps 3 and 4 for the other XBee. If using two computers, repeat them in the other PC. If using only one computer, the consoles will be seen in two tabs. Click the Detach view button to see both at the same time.

PTM פורסם ב: