Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Digi Network Failover Solutions Slide 8

Digi offers several connectivity solutions. The Digi Remote Manager platform is a centralized and secure device-management solution that helps monitor the status of the customers Digi TransPort router and its connection status with real-time alerts, reports and statistics. Like all Digi software, Digi Remote Manager® is PCI-compliant, and serves as a window into out-of-band management. Digi license-free, out-of-band management provides reliable access to the Digi device, even if the network stack or user interface is down. Although it does not replace in-band management, it lets the customer respond faster when standard tools are unavailable. Additionally, Digi takes the Virtual Router Redundancy Protocol (VRRP+) one step further by sending a probe from the Digi TransPort router to an IP address at a remote location. This enables Digi to provide both logical and physical redundancy and failover, based on the status of connections behind the router.

PTM פורסם ב: