Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Enabling Remote Devices Overview Slide 13

The Rabbit 6000 processor adds much stronger communications performance on the RCM6700 MiniCores by increasing the throughput of Rabbit networking modules by an average of five times more than previous Rabbit networking modules. In addition, the modules support remote firmware updates as well as battery backed RAM which were two distinct features not present on the previous MiniCore versions. Dynamic C 10.64 contains a plethora of samples and libraries which essentially completes nearly 80% of an application’s source code, if not more, thus shortening the development effort and reducing time to market.

PTM פורסם ב: