Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Mapping a Digi XBee IoT Network with Digi XCTU Slide 18

There are several ways to scan Digi XBee networks, and these depend on the protocol being used. Small Zigbee networks can be quickly discovered in “flood” mode. Larger ones and DigiMesh networks are better explored with “cascade” mode to avoid saturating the network with requests. Cascade mode is slower. Other timings can also be adjusted, though the defaults should work well in most cases.

PTM פורסם ב: